SDRAM Clocking!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDRAM Clocking!

Jump to solution
650 Views
qammarabbas
Contributor IV

Hi,

I am interfacing 8 DDR3L devices with T1042. The external pin description of T1042 DDR Controller mentions 2 clocks MCK0 and MCK1. Why is there a second clock? Can't i drive all 8 SDRAM devices with a single clock only? 

Tags (1)
0 Kudos
Reply
1 Solution
529 Views
ufedor
NXP Employee
NXP Employee

> Can't i drive all 8 SDRAM devices with a single clock only?

Driving all SDRAM devices connected to the same chip-select with a single/same MCKn is a must.

Please refer to the AN3940 - Hardware and Layout Design Considerations for DDR3 SDRAM, Table 1. DDR3 designer checklist:

"46. Ensure one clock pair is used for each chip-select. The clock pair should follow the address/command/control signal groups in fly-by topology."

View solution in original post

0 Kudos
Reply
1 Reply
530 Views
ufedor
NXP Employee
NXP Employee

> Can't i drive all 8 SDRAM devices with a single clock only?

Driving all SDRAM devices connected to the same chip-select with a single/same MCKn is a must.

Please refer to the AN3940 - Hardware and Layout Design Considerations for DDR3 SDRAM, Table 1. DDR3 designer checklist:

"46. Ensure one clock pair is used for each chip-select. The clock pair should follow the address/command/control signal groups in fly-by topology."

0 Kudos
Reply