SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK

3,576件の閲覧回数
raghavendrasurp
Contributor II

Hi All,

hi im new to this QorIQ LS1043A platform so please send me the SDK (drivers)source code link.

Thanks

Raghavendra

0 件の賞賛
返信
5 返答(返信)

3,403件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please download full Lunix SDK, including source codes, from our Lunux SDK product page:

Linux® SDK for QorIQ Processors|NXP 


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,403件の閲覧回数
raghavendrasurp
Contributor II

Hi Alexander sir,

When i Powered ON my device it took 2.6A current

and when i did REBOOT it took 1.5A current, So whats the reason?

Thanks,

Raghavendra

On Tue, Jan 10, 2017 at 9:17 AM, Raghavendra Surpur <

0 件の賞賛
返信

3,403件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Sorry, what you exactly mean by "my device"?

As far as I remember, the root question of this topic is where to download SDK for LS1043A.

0 件の賞賛
返信

3,403件の閲覧回数
raghavendrasurp
Contributor II

No actually we are working on other platform AM5728 from Texas Instrument

and we have build evaluation board including SATA, SPI, I2C, UART and PCIe

protocols and ours is Media Server Gateway Project, 2 WiFi cards.

We are using Ubuntu 12.04 when i power on the device it took 2.6A but when

did reboot it shown only 1.5A, So whats the reason.

Thanks,

Raghavendra

On Tue, Jan 10, 2017 at 9:43 AM, alexander.yakovlev <[email protected]

0 件の賞賛
返信

3,403件の閲覧回数
raghavendrasurp
Contributor II

thanks

On Sat, Jan 7, 2017 at 4:43 PM, alexander.yakovlev <[email protected]>

0 件の賞賛
返信