Remote power-up on T1040D4-RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Remote power-up on T1040D4-RDB

ソリューションへジャンプ
2,340件の閲覧回数
ricardofranca
Contributor III

Hello,

I have just started tinkering with a T1040D4-RDB and, seeing that it has a power button (unlike an older P1020RDB which had an 1-0 switch), I wonder how I could turn it on remotely. I can activate and deactivate its power socket remotely (which was enough for turning on, off and resetting the older board), but this alone would not turn the board on.

What is the simplest way of doing this?

EDIT: Having removed the board cover, I noticed jumper pins for PWR (J39) and RST (J38), which are described in T1040D4RDBRM as "remote power/reset switches". A friend of mine (who, unlike me, works with electronics) took a look at some diagrams and thinks we cannot simply insert a jumper on J39, as we must generate a pulse there to turn the board on. Is that right?

Thanks!

Ricardo

 

0 件の賞賛
返信
1 解決策
2,228件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Yes, that is right.

You could use PWR (J39) and RST (J38), and a pulse relay is required.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,209件の閲覧回数
ricardofranca
Contributor III

Thanks! I do not know if I should open a separate thread for another question: What is the CPLD address I should write in order to operate the status LED and the board fan? I thought it should be 0xffdf0014 but nothing happens when I change values there.

0 件の賞賛
返信
2,153件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please address your new question in a new thread.

0 件の賞賛
返信
2,229件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Yes, that is right.

You could use PWR (J39) and RST (J38), and a pulse relay is required.

0 件の賞賛
返信