Query regarding P5040 Frame manager clock select RCW bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Query regarding P5040 Frame manager clock select RCW bit

1,605 Views
ramchet
Contributor I

In the P5040 reference manual Document Number: P5040RM Rev. 3, 6/2016, Table 4-10 states that when Frame manager clock select RCW bit(225 and 226) is set as ‘1’,  FM clock will be “ Core cluster 3 PLL/2 or /4”.  Please clarify when this bit is set as "1" what will be the frame manager clock?  Will it be Core cluster 3 PLL/2 OR Core cluster 3 PLL/4. Please see the attached snapshot

0 Kudos
Reply
1 Reply

1,532 Views
ufedor
NXP Employee
NXP Employee

Please refer to the RCW bit 229 description.

0 Kudos
Reply