Query regarding P1013 processor interfacing with 16 bit DDR3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Query regarding P1013 processor interfacing with 16 bit DDR3

791 次查看
lokeshe
Contributor I

We are Using P1013 power PC processor and we need to interface 16 bit DDR3 memory. But as per the P1013 datasheet it say it can support only 32/64 bit. Can you pleasd confirm if we can interface single 16 bit DDR3 with processor or we have to use two 16 bit DDR3.

0 项奖励
回复
1 回复

746 次查看
r8070z
NXP Employee
NXP Employee

Have a great day,

The P1013 DDR controller does not support 16-bit SDRAM data bus. It requires at least for two 16-bit DDR3 memory devices.

The P1010/P1014 support 16-bit DDR3 SDRAM data bus.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复