Query about LS1043A Toolchain.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Query about LS1043A Toolchain.

1,780件の閲覧回数
maheshbalasubr1
Contributor II

Hi,

LS1043ARDB seems to be based on Cortex-A53 processor with ARMv8-A architecture.  Whereas the linux toolchain provided by NXP appears to be Cortex-A7 architecture.  I understand Cortex-A53 has backwards compatibility architecture.

I was checking if there is any option to use a toolchain that supports ARMV8-A instruction set?

Thanks,

1 返信

1,709件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers Yocto Linux BSP SDK 2.7 for the LS1043a:

https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/about/

 

Use toolchain from this SDK.

 

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------