QoIrq T1042 RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QoIrq T1042 RDB

1,971件の閲覧回数
weizhao
Contributor I

Hi,

We are intending to use T1042 as our new generation SP card processor, and we'd like to run Freescale embedded Hypervisor on it.  Above Hypervisor there will be two OS running, Linux 4.1 and VxWorks 6.9.  Can you please tell me if there is a T1042 RDB to purchase ? If there is one, can you please send me the web page to get more information about the board ?  Also can you please provide some information on which SDK version supports T1042 ?

Thank.

0 件の賞賛
返信
1 返信

1,576件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

I see on the nxp T1042RDB part details page https://www.nxp.com/webapp/webapp/search.partparamdetail.framework?PART_NUMBER=T1042RDB-PA   that it has
Life Cycle Description (code) = REMOVED FROM ACTIVE PORTFOLIO
Status = No Longer Manufactured
Possibly some distributors (Arrow, Digikey, etc…) may still have it for sale.

There is T1040RDB which also support the T1042
http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-plat...

For the Hypervisor and supported SDK start from
http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-plat...

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信