QCVS (PA) Installation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

QCVS (PA) Installation

跳至解决方案
3,916 次查看
ralftruebenbach
Contributor III

Hello,

I'm trying to install the QorIQ Configuration and Validation Suite (for PowerPC T2080).

1) In QCVS_Install_Guide.pdf there is an all-in-one installer mentioned but at http://www.freescale.com/qcvs I can only find the offline installation packages for eclipse. Is the all-in-one installer still available?

2) I installed CodeWarrior for Power Architecture 10.5.1. But there is no "QorIQ Configuration Project" in File > New > (only CodeWarrior...ProjectWizard). Did I something wrong during the installation or do I have to install something else?
I also recognised that the "Available Software Sites" are quite empty (only 2 locations from eclipse.org). So I cannot update. Is there an update site for code warrior I can add?

3) I also tried to install the QCVS over my eclipse (online and offline) as described in "3.2 Installation over Eclipse" ending up with the error below. I think this is because my eclipse version 4.4 (Luna) is > 4.2?

An error occurred while installing the items
session context was:(profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Install, operand=null --> [R]com.freescale.qcvs.feature_root 4.5.0.0001-20160210, action=com.freescale.updater.customactions.actions.FreescaleProcessCheck).
org/eclipse/core/runtime/adaptor/LocationManager
org/eclipse/core/runtime/adaptor/LocationManager

标记 (2)
0 项奖励
回复
1 解答
2,945 次查看
ralftruebenbach
Contributor III

2) I reinstalled "CodeWarrior for Power Architecture 10.5.1". This time I can see Freescale related update sites in "Available Software Sites" and installing the offline QCVS packages works (did not work with last installation).

3) I think that's what I did. Eclipse lists "FSL Eclipse Updater Custom Actions Feature for Eclipse 3.7 and 4.2.x..." at installed Software. But I don't care anymore since 2) worked. I didn't try with a fresh Eclipse 4.2 installation (most likely that would work, too).

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,945 次查看
ufedor
NXP Employee
NXP Employee

1) No,

2) It is possible to install the QCVS from the offline installation packages for CodeWarrior:

https://nxp.flexnetoperations.com/control/frse/download?element=6979427 

3) The installation of QCVS relies on a Freescale Eclipse updater feature. This feature is not part of Eclipse stock distributions, but is bundled with CodeWarrior. For this reason, the installation of QCVS over an Eclipse other than CodeWarrior requires that you first install the Eclipse Updater feature:

Submit Form 

0 项奖励
回复
2,946 次查看
ralftruebenbach
Contributor III

2) I reinstalled "CodeWarrior for Power Architecture 10.5.1". This time I can see Freescale related update sites in "Available Software Sites" and installing the offline QCVS packages works (did not work with last installation).

3) I think that's what I did. Eclipse lists "FSL Eclipse Updater Custom Actions Feature for Eclipse 3.7 and 4.2.x..." at installed Software. But I don't care anymore since 2) worked. I didn't try with a fresh Eclipse 4.2 installation (most likely that would work, too).

0 项奖励
回复