Problems Building 1043A (fsl-image-x11) Source not found error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems Building 1043A (fsl-image-x11) Source not found error

Jump to solution
2,992 Views
donberkowitz
Contributor II

Hi,

I did the above build using the 0.5 source toolchain, all but one task ran successfully, but one task continues to fail.  The log is below.  Any ideas on what is wrong would be greatly appreciated.

Thanks!!!!

Don

NOTE: Preparing runqueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: Function failed: do_compile (log file is located at /home/don/Linux-LS1043A-SDK-V0.5-20151223-yocto/build_ls1043ardb_release/tmp/work/ls1043ardb-fsl-linux/uefi-ls1043a/git-r0/temp/log.do_compile.5226)
ERROR: Logfile of failure stored in: /home/don/Linux-LS1043A-SDK-V0.5-20151223-yocto/build_ls1043ardb_release/tmp/work/ls1043ardb-fsl-linux/uefi-ls1043a/git-r0/temp/log.do_compile.5226
Log data follows:
| DEBUG: Executing shell function do_compile
| /home/don/Linux-LS1043A-SDK-V0.5-20151223-yocto/build_ls1043ardb_release/tmp/work/ls1043ardb-fsl-linux/uefi-ls1043a/git-r0/temp/run.do_compile.5226: 101: /home/don/Linux-LS1043A-SDK-V0.5-20151223-yocto/build_ls1043ardb_release/tmp/work/ls1043ardb-fsl-linux/uefi-ls1043a/git-r0/temp/run.do_compile.5226: source: not found
| WARNING: exit code 127 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/don/Linux-LS1043A-SDK-V0.5-20151223-yocto/build_ls1043ardb_release/tmp/work/ls1043ardb-fsl-linux/uefi-ls1043a/git-r0/temp/log.do_compile.5226)
ERROR: Task 95 (/home/don/Linux-LS1043A-SDK-V0.5-20151223-yocto/meta-fsl-networking/recipes-bsp/uefi/uefi-ls1043a_git.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2732 tasks of which 2729 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:

Summary: 1 task failed:
  /home/don/Linux-LS1043A-SDK-V0.5-20151223-yocto/meta-fsl-networking/recipes-bsp/uefi/uefi-ls1043a_git.bb, do_compile
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
don@don-LTJ843:~/Linux-LS1043A-SDK-V0.5-20151223-yocto/build_ls1043ardb_release$ bitbake fsl-image-x11

0 Kudos
Reply
1 Solution
2,224 Views
lunminliang
NXP Employee
NXP Employee

Hello Don Berkowitz,

There is issue of UEFI build in dash environment. You can change the default shell to bash and try again. I can build succesfully on Ubuntu 14.04 with V03. Below are my steps:

freescale@freescale-sdk:~/Linux-LS1043A-SDK-V0.3-20150729-yocto/build_ls1043ardb_release$ ls -l /bin/sh

lrwxrwxrwx 1 root root 4 Jul  2  2014 /bin/sh -> dash

freescale@freescale-sdk:~/Linux-LS1043A-SDK-V0.3-20150729-yocto/build_ls1043ardb_release$ sudo dpkg-reconfigure dash

Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'

Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'

Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'

Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'

freescale@freescale-sdk:~/Linux-LS1043A-SDK-V0.3-20150729-yocto/build_ls1043ardb_release$ ls -l /bin/sh

lrwxrwxrwx 1 root root 4 Aug 17 16:07 /bin/sh -> bash

freescale@freescale-sdk:~/Linux-LS1043A-SDK-V0.3-20150729-yocto/build_ls1043ardb_release$ bitbake fsl-image-kernelitb

Loading cache: 100% |###########################################| ETA:  00:00:00

Loaded 2010 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.22.0"

BUILD_SYS        = "i686-linux"

NATIVELSBSTRING  = "Ubuntu-14.04"

TARGET_SYS        = "aarch64-fsl-linux"

MACHINE          = "ls1043ardb"

DISTRO            = "fsl-networking"

DISTRO_VERSION    = "1.6.1"

TUNE_FEATURES    = "aarch64"

meta            

meta-yocto      

meta-yocto-bsp    = "(detachedfromee91d21):error:"

meta-fsl-arm      = "(detachedfrom9400922):error:"

meta-fsl-networking = "(detachedfromd489088):error:"

meta-fsl-toolchain

meta-virtualization = "<unknown>:<unknown>"

meta-oe        

meta-networking

meta-perl      

toolchain-layer  = "(detachedfrome0bb767):<unknown>"

meta-linaro-toolchain = "(detachedfrom6452ef4):error:"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

NOTE: Tasks Summary: Attempted 2424 tasks of which 2148 didn't need to be rerun and all succeeded.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,225 Views
lunminliang
NXP Employee
NXP Employee

Hello Don Berkowitz,

There is issue of UEFI build in dash environment. You can change the default shell to bash and try again. I can build succesfully on Ubuntu 14.04 with V03. Below are my steps:

freescale@freescale-sdk:~/Linux-LS1043A-SDK-V0.3-20150729-yocto/build_ls1043ardb_release$ ls -l /bin/sh

lrwxrwxrwx 1 root root 4 Jul  2  2014 /bin/sh -> dash

freescale@freescale-sdk:~/Linux-LS1043A-SDK-V0.3-20150729-yocto/build_ls1043ardb_release$ sudo dpkg-reconfigure dash

Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'

Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'

Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'

Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'

freescale@freescale-sdk:~/Linux-LS1043A-SDK-V0.3-20150729-yocto/build_ls1043ardb_release$ ls -l /bin/sh

lrwxrwxrwx 1 root root 4 Aug 17 16:07 /bin/sh -> bash

freescale@freescale-sdk:~/Linux-LS1043A-SDK-V0.3-20150729-yocto/build_ls1043ardb_release$ bitbake fsl-image-kernelitb

Loading cache: 100% |###########################################| ETA:  00:00:00

Loaded 2010 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.22.0"

BUILD_SYS        = "i686-linux"

NATIVELSBSTRING  = "Ubuntu-14.04"

TARGET_SYS        = "aarch64-fsl-linux"

MACHINE          = "ls1043ardb"

DISTRO            = "fsl-networking"

DISTRO_VERSION    = "1.6.1"

TUNE_FEATURES    = "aarch64"

meta            

meta-yocto      

meta-yocto-bsp    = "(detachedfromee91d21):error:"

meta-fsl-arm      = "(detachedfrom9400922):error:"

meta-fsl-networking = "(detachedfromd489088):error:"

meta-fsl-toolchain

meta-virtualization = "<unknown>:<unknown>"

meta-oe        

meta-networking

meta-perl      

toolchain-layer  = "(detachedfrome0bb767):<unknown>"

meta-linaro-toolchain = "(detachedfrom6452ef4):error:"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

NOTE: Tasks Summary: Attempted 2424 tasks of which 2148 didn't need to be rerun and all succeeded.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,224 Views
olegnazarov
Contributor I

I would also add that this error is easily reproduced on a freshly installed Xubuntu 14.04, while the CentOS 7.2 builds the image just fine.

$ uname -a

Linux yacht 3.19.0-25-generic #26~14.04.1-Ubuntu SMP Fri Jul 24 21:16:20 UTC 2015 x86_64 x86_64 x86_64 GNU/Linux

P.S.

After some investigation, the solution appears to be very simple. It appears that the ubuntu links /bin/sh to /bin/dash shell. As the build scripts rely on that the /bin/sh is actually /bin/bash, they use source directive extensively. For dash shell that does not work.

So to resolve the issue:

$ sudo rm /bin/sh

$ sudo ln -s /bin/bash /bin/sh

0 Kudos
Reply