Problem in Root File System Mount

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem in Root File System Mount

2,010件の閲覧回数
leelambjae
Contributor I

Hi 

We are trying to do a secure booting in T2080RDB-PC.

 

We saved the image and csf header in NOR Altbank(vbank 4) and confirmed that validate part(esbc_validate) print 'Successful'

However, root file system is not mounted. Can you find answer to this question?

We attach our consol , ubootenv, and the filename which we used for the secure booting demo.

In addition, we trying to change ubootenv, but confirmed that secure u-boot dose not support saveenv.

Thank You.

alterbank.png

this is error screenshot.

baudrate=115200
bdev=sda3
bootcmd=setenv bs_hdraddr 0xe8e00000;setenv bootargs 'root=/dev/ram rw console=ttyS0,115200 ramdisk_size=600000';esbc_validate $bs_hdraddr;source $img_addr;esbc_halt
bootdelay=0
bootfile=uImage
consoledev=ttyS0
ethact=FM1@DTSEC3
ethprime=FM1@DTSEC3
fdtaddr=1e00000
fdtfile=t2080rdb/t2080rdb.dtb
fman_ucode=eff00000
hwconfig=fsl_ddr:ctlr_intlv=cacheline,bank_intlv=auto;usb1:dr_mode=host,phy_type=utmi
initrd_high=0xffffffff
loadaddr=1000000
netdev=eth0
nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:$netdev:off console=$consoledev,$baudrate $othbr
ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootr
ramdiskaddr=2000000
ramdiskfile=t2080rdb/ramdisk.uboot
rootpath=/opt/nfsroot
stderr=serial
stdin=serial
stdout=serial
tftpflash=tftpboot $loadaddr $uboot && protect off $ubootaddr +$filesize && erase $ubootaddr +$filesize && cp.b $loadaddr $ubootaddr $filesize && protect on $ubootaddre
uboot="u-boot.bin"
ubootaddr=0xeff40000

Environment size: 1360/8188 bytes

this is ubootenv.

filename is as follows

U-boot
u-boot-secure-boot-2016.09+fslgit-r0.bin

rootfs
fsl-image-core-t2080rdb-64b-20180717052401.rootfs.ext2.gz.u-boot

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,879件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello yangjae lee,

Please refer to the following memory map for T2080RDB NOR flash, rootfs is allocated as 29696KB, however the default rootfs ramdisk image provided in the pre-built image ISO is about 31M, please rebuild rootfs image to reduce the size or build fsl-image-minimal image with "bitbake fsl-image-minimal".

pastedImage_2.png


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,879件の閲覧回数
liguofa
Contributor III

The problem is NFS problem ! not addr for nor start .Please Read the question first ,thanks

0 件の賞賛
返信