Hello, everyone.
I did connect to P4080 through minicom for uploading RCW, u-boot, Kernel, Ramdisk image.
When the ramdisk image copy process had been completed, minicom wasn't interacting suddenly.
So I tried to quit and re-execute a minicom but it is not interacting like attached image file.
Please help me.
How could I re-connect to P4080 through minicom?
If the fully-reset solution for P4080 exists?
Thank you.
Okay, I will try the approach you said.
Thank you for persistently contributing to me.
I didn't know that I need CodeWarrior TAP.
No, I don't have. If I don't have CodeWarrior TAP, I couldn't solve this problem?
Thank you.
But I haven't an experience for CodeWarrior Flash Programmer so that may be hard challenge for me.
Could you give me a manual or simple description to program pre-compiled NOR flash image using CodeWarrior?
So you have CodeWarrior IDE installed, CodeWarrior TAP and PA Probe Tip connected to the JTAG connector of the P4080DS board?
In this case it is recommended to use CodeWarrior Flash Programmer to program pre-compiled NOR Flash image provided in the ISO "QorIQ Linux SDK v2.0 PPCE500MC IMAGE":