Problem dumping NOR flash memory on LS1021A-TWR board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem dumping NOR flash memory on LS1021A-TWR board

1,736 Views
jayarajrajappan
Contributor II

I'm using LS1021A-TWR board. I'm booting from SD card and trying to dump the NOR flash memory using "md" command. However, I'm getting the following unexpected values. How do I recover the NOR flash from this?

Also, is there a way to reset the board to the factory default settings?

=> md 60000000

00000000: e59ff018 e59ff018 e59ff018 e59ff018 ................

00000010: e59ff018 e59ff018 e59ff018 e59ff018    ................

00000020: 00001ec0 0000180c 00001850 00001894    ........P.......

00000030: 000018d8 0000191c 00001960 000019a4    ........`.......

00000040: 45535546 54544120 00000052 52545023    FUSE ATTR...#PTR

00000050: 00000000 4f525245 20202052 00000000    ....ERROR   ....

00000060: 54495257 004e4554 6d697250 676d4920    WRITTEN.Prim Img

00000070: 69616620 6572756c 00000000 20636553     failure....Sec

00000080: 20676d49 69676562 0000006e 616e6946    Img begin...Fina

00000090: 7245206c 20726f72 00202020 65736552    l Error    .Rese

000000a0: 00000074 52424924 0000005f 70657453    t...$IBR_...Step

000000b0: 20202031 00000000 204d554e 00434553    1   ....NUM SEC.

000000c0: 70657453 20202032 00000000 70657453    Step2   ....Step

000000d0: 20202033 00000000 70657453 20202035    3   ....Step5

000000e0: 00000000 70657453 20202036 00000000    ....Step6   ....

000000f0: 70657453 20202037 00000000 70657453    Step7   ....Step

2 Replies

1,646 Views
sinanakman
Senior Contributor III

Hi Jayaraj

If your NOR was mistakenly overwritten (perhaps

by another user), you can reprogram your NOR

with the correct image again by using u-boot commands.

Regards

Sinan Akman

0 Kudos
Reply

1,646 Views
jayarajrajappan
Contributor II

Hi,

I figured this out. It was not a case of my NOR getting overwritten. For some reason, due to the RCW that I was using to boot from SD card, PBL didn't seem to have initialized the IFC, which was causing this issue. Once I used a good image (u-boot-with-spl-pbl.bin) with a proper RCW to boot from SD, I was able to dump the contents of the NOR flash correctly.

Thanks.