Power Consumption onf LS1012A Development Boards

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Power Consumption onf LS1012A Development Boards

跳至解决方案
1,866 次查看
joe1652
Contributor IV

Hello, I am looking for design a board using the LS1012A ARM processor. I am looking at my power requirements and have a question that I hope someone can help me with. According to the documentation on the XFRWY-LS101A-PA Rev-B board the power consumption is 16W at 1A. Is there any information on how much current the board is consuming on the 0.9V, 1.35V, 1.8V and the 2.5V rails? I need this to determine if I will need a heat sink on my input regulator. My input voltage is 18V so I need to find a regulator that won't get too hot.

Thanks,

Joe

1 解答
1,793 次查看
ufedor
NXP Employee
NXP Employee

Power consumption of the XFRWY-LS1012A:

Supply [V]Max. Current [A]
3.33.2
1.80.4
1.350.6
0.91.35

2.5V - not used.

在原帖中查看解决方案

1 回复
1,794 次查看
ufedor
NXP Employee
NXP Employee

Power consumption of the XFRWY-LS1012A:

Supply [V]Max. Current [A]
3.33.2
1.80.4
1.350.6
0.91.35

2.5V - not used.