Power Consumption onf LS1012A Development Boards

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power Consumption onf LS1012A Development Boards

Jump to solution
1,868 Views
joe1652
Contributor IV

Hello, I am looking for design a board using the LS1012A ARM processor. I am looking at my power requirements and have a question that I hope someone can help me with. According to the documentation on the XFRWY-LS101A-PA Rev-B board the power consumption is 16W at 1A. Is there any information on how much current the board is consuming on the 0.9V, 1.35V, 1.8V and the 2.5V rails? I need this to determine if I will need a heat sink on my input regulator. My input voltage is 18V so I need to find a regulator that won't get too hot.

Thanks,

Joe

1 Solution
1,795 Views
ufedor
NXP Employee
NXP Employee

Power consumption of the XFRWY-LS1012A:

Supply [V]Max. Current [A]
3.33.2
1.80.4
1.350.6
0.91.35

2.5V - not used.

View solution in original post

1 Reply
1,796 Views
ufedor
NXP Employee
NXP Employee

Power consumption of the XFRWY-LS1012A:

Supply [V]Max. Current [A]
3.33.2
1.80.4
1.350.6
0.91.35

2.5V - not used.