P5020NSE7MMB processor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P5020NSE7MMB processor?

1,056 Views
chockkalingamm
Contributor I

We are using this processor P5020NSE7MMB one of  the defense  project, let me know the below interface it will support or not and suggest alternate solutions.

1) ARNIC 429 interface 2 Nos

2) CAN interface            2Nos

3) RS 422 interface       4 Nos

4) PWM outputs           10 Nos

5) H bridge driver          10 Nos

Thanks & Regards,

Chockkalingam M#

0 Kudos
Reply
1 Reply

995 Views
alexander_yakov
NXP Employee
NXP Employee

1) ARNIC 429 interface 2 Nos

ARINC429 protocol is not supported by our QorIQ family networking processors.

External third-party controller will be required (if any). Alternatively, you can consider a device from Automotive or Industrial product segments, these devices have “eTPU” block, which may be used to implement ARINC429.

2) CAN interface            2Nos

CAN interface is not supported in P5020 processor, please consider another device – for example P1010 or LS1021A.

3) RS 422 interface       4 Nos

RS422 is “electrical” standard, typically UART with RS422 transceivers is used. Yes, UART is supported.

4) PWM outputs           10 Nos

PWM is not supported by P5020 processor, please consider another devices with Flex Timer module, for example LS1021A or later Layerscape devices.

5) H bridge driver          10 Nos

H-bridge is not supported in Networking products, please consider device from Automotive or Motor Control product segments.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply