P2020 Processor TEPBGA2 Package Construction

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020 Processor TEPBGA2 Package Construction

Jump to solution
1,880 Views
ethan135
Contributor II

Xilinx's App note XAPP426 indicates they intentionally design in vents between the package's heatspreader (lid) and the organic substrate. Does the P2020 Processor also have these vents designed into its TEPBGA2 package, or is the lid hermetically sealed with the substrate?

0 Kudos
Reply
1 Solution
1,812 Views
andrei_skok
NXP Employee
NXP Employee

P2020 has small vent holes between the lid and the organic substrate to allow for outgassing and moisture evaporation.


Have a great day,
Andrei

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,813 Views
andrei_skok
NXP Employee
NXP Employee

P2020 has small vent holes between the lid and the organic substrate to allow for outgassing and moisture evaporation.


Have a great day,
Andrei

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------