P2020 Processor Connecting Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P2020 Processor Connecting Issue

978 次查看
rajeshkp
Contributor I

​Iam using P2020 Q or IQ Processor if iam trying to connect the processor through Code warrior its not connecting actually it goes to running  state.Unable to check or program processor.JTAG signals & reset condition i have checked all in normal only.So give suggestions solve this issue.

0 项奖励
回复
1 回复

826 次查看
ufedor
NXP Employee
NXP Employee

It is required to check the following points:

1) refer to the P2020 Hardware Specification and check that all notes after the Table 1. Pin List by Bus are fulfilled.

Pay special attention to the Note 15 and use a digital scope to check the signals behaviour during power-on.

2) ensure that the processor POR behaviour is as described in the P2020 QorIQ Integrated Processor Reference Manual, 4.5.2 Power-on reset sequence.

If these checkings do not help please consider open a technical case to investigate the issue in more detail.

How I could create a Service Request?

0 项奖励
回复