P1020RDB-PD boot from either Flash or SD card.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1020RDB-PD boot from either Flash or SD card.

795件の閲覧回数
dennis_l_bergin
Contributor I

I am looking to boot the P1020RDB-PD from either Flash or SD card.  I would like to try both.  Ultimately, I would like to have a bootable image with VxWorks kernel and application.  Can you point me to documentation and boot images to do this?

Thanks
Dennis

0 件の賞賛
返信
1 返信

717件の閲覧回数
ufedor
NXP Employee
NXP Employee

The QorIQ SDK V1.9 PPCE500V2 IMAGE ISO contains following pre-built binary images for the P1020RDB-PD:

U-Boot NOR image, U-Boot SD card image, complete NOR Flash image and complete NAND Flash image

The ISO can be downloaded from:

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7126427

Concerning VxWorks images and their deployment please contact Wind River directly.

0 件の賞賛
返信