P1020 eTSEC CPU CRITICAL BUG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1020 eTSEC CPU CRITICAL BUG

2,141 Views
ivanlukyanchuk
Contributor I

Hello!

History of analisys of problem is here https://community.freescale.com/message/653136. Because problem is very important, I create new question thread.

I find bug in P1020 eTSEC controller.

Problem: eTSEC put to RxBDs ring previous packet, not last received.

Method that activate the problem: We connect from one PC to device 2 way. 1. Ping. 2. Cyclic download files from device to PC. We restart device every 20-30 min, and problem is activated several times during one day.

Using software: linux QorIQ SDK 1.9

 

I add debug to gianfar, and see that ETSEC put to RxBDs ring only previous packet, not last received. I send to device various length packets, log bdp->lstatus (in gfar_clean_rx_ring())  for current and next BDP and see this behaviour very well.

 

Problem occurs when eTSEC packet parser is enabled (RCTRL[PRSDEP]=0x11). When eTSEC packet parser is disabled (RCTRL[PRSDEP]=0x0)? problem not occurs. Problem not depend on filer. Problem occurs when filer is enabled (RCTRL[FILEN]=1) or disabled (RCTRL[FILEN]=0).

 

Registers state after problem is occured.

root@p1020rdb:~# ethtool -d eth0

Offset          Values

------          ------

0x0000:         01 24 02 00 00 ee 00 f0 00 00 00 00 00 00 00 00

0x0010:         00 00 00 00 f1 31 00 83 00 00 00 00 00 00 00 00

0x0020:         00 00 10 0c 00 00 00 00 00 00 00 04 00 00 00 c3

0x0030:         00 00 00 1f 00 00 00 00 00 00 00 00 00 00 00 00

0x0040:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0050:         00 00 00 80 00 00 00 c0 00 00 00 40 00 00 00 80

0x0060:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0070:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0080:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 01 00

0x0090:         00 00 00 00 00 00 00 00 00 00 00 40 00 00 00 80

0x00a0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x00b0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x00c0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x00d0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x00e0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x00f0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0100:         00 00 60 02 80 00 80 00 81 00 00 00 00 00 00 00

0x0110:         82 00 00 15 00 00 80 00 00 00 00 00 00 00 00 00

0x0120:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0130:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0140:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0150:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0160:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0170:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0180:         00 00 00 00 17 45 02 60 00 00 00 00 00 00 00 00

0x0190:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x01a0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x01b0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x01c0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x01d0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x01e0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x01f0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0200:         00 00 00 00 17 45 00 00 00 00 00 00 00 00 00 00

0x0210:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0220:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0230:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0240:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0250:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0260:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0270:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0280:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0290:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x02a0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x02b0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x02c0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x02d0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x02e0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x02f0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0300:         00 08 77 c2 02 00 00 80 00 00 00 00 00 00 00 00

0x0310:         00 00 00 00 00 80 00 80 04 10 41 00 00 00 00 00

0x0320:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0330:         00 00 00 00 00 00 00 e6 00 00 00 60 ff ff ff ff

0x0340:         00 00 06 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0350:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0360:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0370:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0380:         00 00 00 00 17 45 0b 08 00 00 00 00 00 00 00 00

0x0390:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x03a0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x03b0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x03c0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x03d0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x03e0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x03f0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0400:         00 00 00 00 17 45 08 00 00 00 00 00 00 00 00 00

0x0410:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0420:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0430:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0440:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0450:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0460:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0470:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0480:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0490:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x04a0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x04b0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x04c0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x04d0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x04e0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x04f0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0500:         00 00 00 0f 00 00 71 05 40 60 50 60 00 a1 f0 37

0x0510:         00 00 06 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0520:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0530:         00 00 00 00 00 00 00 00 01 00 00 00 00 00 00 00

0x0540:         00 40 04 c5 1b 00 00 00 01 00 00 5e 00 01 00 00

0x0550:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0560:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0570:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0580:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0590:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x05a0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x05b0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x05c0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x05d0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x05e0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x05f0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0600:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0610:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0620:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0630:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0640:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0650:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0660:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0670:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0680:         00 01 5e ac 00 00 d2 9d 00 00 19 7c 00 00 0f 17

0x0690:         00 00 12 af 00 03 64 a8 00 00 00 00 00 90 09 7c

0x06a0:         00 02 04 33 00 00 01 42 00 00 00 57 00 00 00 8f

0x06b0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x06c0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x06d0:         00 00 00 00 00 00 11 be 00 00 00 00 00 00 00 5e

0x06e0:         10 93 18 a5 00 03 de be 00 00 00 00 00 00 00 00

0x06f0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0700:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0710:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0720:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0730:         00 00 00 00 00 00 00 00 fe 03 ff ff 00 0f ff fd

0x0740:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0750:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0760:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0770:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0780:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0790:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x07a0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x07b0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x07c0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x07d0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x07e0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x07f0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0800:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0810:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0820:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0830:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0840:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0850:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0860:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0870:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0880:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0890:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x08a0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x08b0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x08c0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x08d0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x08e0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x08f0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0900:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0910:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0920:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0930:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0940:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0950:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0960:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0970:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0980:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0990:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x09a0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x09b0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x09c0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x09d0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x09e0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x09f0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0a00:         00 00 00 c0 00 00 00 00 00 00 00 00 00 00 00 00

0x0a10:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0a20:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0a30:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0a40:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0a50:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0a60:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0a70:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0a80:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0a90:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0aa0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0ab0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0ac0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0ad0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0ae0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0af0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0b00:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0b10:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0b20:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0b30:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0b40:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0b50:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0b60:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0b70:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0b80:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0b90:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0ba0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0bb0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0bc0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0bd0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0be0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0bf0:         00 00 00 00 00 00 00 00 00 00 48 c0 00 60 00 00

0x0c00:         10 00 01 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0c10:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0c20:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0c30:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0c40:         00 00 00 00 17 45 08 00 00 00 00 00 00 00 00 00

0x0c50:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0c60:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0c70:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0c80:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0c90:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0ca0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0cb0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0cc0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0cd0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0ce0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0cf0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0d00:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0d10:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0d20:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0d30:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0d40:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0d50:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0d60:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0d70:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0d80:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0d90:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0da0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0db0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0dc0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0dd0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0de0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0df0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0e00:         00 01 00 01 00 00 00 00 00 00 00 00 00 00 00 00

0x0e10:         00 00 00 00 80 00 00 00 00 00 00 00 00 00 00 00

0x0e20:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0e30:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0e40:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0e50:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0e60:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0e70:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0e80:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0e90:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0ea0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0eb0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0ec0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0ed0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0ee0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0ef0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0f00:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0f10:         82 00 00 15 00 00 00 00 00 00 00 00 00 00 00 00

0x0f20:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0f30:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0f40:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0f50:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0f60:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0f70:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0f80:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0f90:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0fa0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0fb0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0fc0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0fd0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0fe0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

0x0ff0:         00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

Original Attachment has been moved to: radius_oe.dts.zip

Original Attachment has been moved to: 1.pcap.zip

Original Attachment has been moved to: radius_defconfig.zip

0 Kudos
Reply
3 Replies

1,850 Views
ivanlukyanchuk
Contributor I

Case 00078788

0 Kudos
Reply

1,850 Views
ivanlukyanchuk
Contributor I

Case 00078213

Are you speak russian? May be you call me by phone or skype (workvguard007)?

Regards,

Ivan

0 Kudos
Reply

1,850 Views
bpe
NXP Employee
NXP Employee

The issue you are describing doesn't look typical. It's analysis and discussion it is likely

to require long time,  exchanging large amounts of information and possibly NDA documentation and/or

details of your hardware design which is not appropriate for a public forum. For this reason, may I suggest that you

create a Support Case for it?

Details on how to create Support Cases can be found here:

https://community.nxp.com/docs/DOC-329745

Regards,

Platon

0 Kudos
Reply