P1010, eTSEC, Buffer Descriptor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1010, eTSEC, Buffer Descriptor

ソリューションへジャンプ
2,906件の閲覧回数
annettekratz
Contributor I

I have a problem with P1010 and Ethernet Communication. I configured a ring with 16 BDs. When I activate 1 BD to send data, nothing happens, just TBPTR0 jumps to the next BD. When the ring is full, all 0x8000-Bits are cleared and TBPTR0 jumps to  1. BD. The data is never send, also no error information in BD received. What could be the reason?

タグ(1)
0 件の賞賛
返信
1 解決策
2,751件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,752件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
2,751件の閲覧回数
bpe
NXP Employee
NXP Employee

Well, if you see R bits cleared, it means the BDs have been processed.

Either, there are error indications in IEVENT or BDs, or the frames have been

sent out. For the single ready BD case, looks like a memory coherency

issue. Suggestions:

1. Make sure you are using physical, not virtual addresses for any eTSEC

DMA related pointers.

2. Make sure TxBD are 8-byte aligned

3. Make sure DMACTRL[TDSEN, TBDSEN] are set.

4. Set MACCFG1[Loop_Back], RCTRL[PROM] and see if anything is received

   in the MAC loopback mode and/or any counter is updated.

  


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信