P1010, eTSEC, Buffer Descriptor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1010, eTSEC, Buffer Descriptor

Jump to solution
2,910 Views
annettekratz
Contributor I

I have a problem with P1010 and Ethernet Communication. I configured a ring with 16 BDs. When I activate 1 BD to send data, nothing happens, just TBPTR0 jumps to the next BD. When the ring is full, all 0x8000-Bits are cleared and TBPTR0 jumps to  1. BD. The data is never send, also no error information in BD received. What could be the reason?

Tags (1)
0 Kudos
Reply
1 Solution
2,755 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
2,756 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
2,755 Views
bpe
NXP Employee
NXP Employee

Well, if you see R bits cleared, it means the BDs have been processed.

Either, there are error indications in IEVENT or BDs, or the frames have been

sent out. For the single ready BD case, looks like a memory coherency

issue. Suggestions:

1. Make sure you are using physical, not virtual addresses for any eTSEC

DMA related pointers.

2. Make sure TxBD are 8-byte aligned

3. Make sure DMACTRL[TDSEN, TBDSEN] are set.

4. Set MACCFG1[Loop_Back], RCTRL[PROM] and see if anything is received

   in the MAC loopback mode and/or any counter is updated.

  


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply