Option for RTC in P1022 processors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Option for RTC in P1022 processors

1,325 次查看
rachanatm
Contributor II

Hi,

In P1022 processor, Is there in option to keep track of current time?

0 项奖励
回复
1 回复

1,256 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,
 

I am not sure what do you mean as “option to keep track of current time”. The P1022 has timebase and global timer facilities which can be used to implement system time count. But it cannot count when power is off. So it is better to use external real-time clock device with SPI or I2C interface to get/set time. For example P1022RDK board has separate RTC  device (M41T62Q6F) with lithium rechargeable coin battery. It is connected to the P1022 I2C.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复