Option for RTC in P1022 processors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Option for RTC in P1022 processors

1,339件の閲覧回数
rachanatm
Contributor II

Hi,

In P1022 processor, Is there in option to keep track of current time?

0 件の賞賛
返信
1 返信

1,270件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,
 

I am not sure what do you mean as “option to keep track of current time”. The P1022 has timebase and global timer facilities which can be used to implement system time count. But it cannot count when power is off. So it is better to use external real-time clock device with SPI or I2C interface to get/set time. For example P1022RDK board has separate RTC  device (M41T62Q6F) with lithium rechargeable coin battery. It is connected to the P1022 I2C.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信