OHCI context controller active bit doesn't clear

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OHCI context controller active bit doesn't clear

913件の閲覧回数
hv
Contributor II

I'm having a problem running on the T2080 that when I transmit to a PCIe by setting the OHCI context controller run bit, the context controller active bit is set and remains set (never clears!)  The active bit is set and cleared only by the Host Controller. 

Can someone tell me why this is the case?  This piece of code runs fine on the T1040.

thanks!

0 件の賞賛
返信
1 返信

832件の閲覧回数
Pavel
NXP Employee
NXP Employee

The T2080 PCIe and T1040 PCIe are similar controllers. Do you use the same SDK Linux BSP on the T2080 and T1040 boards?

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信