OHCI context controller active bit doesn't clear

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OHCI context controller active bit doesn't clear

409 Views
hv
Contributor II

I'm having a problem running on the T2080 that when I transmit to a PCIe by setting the OHCI context controller run bit, the context controller active bit is set and remains set (never clears!)  The active bit is set and cleared only by the Host Controller. 

Can someone tell me why this is the case?  This piece of code runs fine on the T1040.

thanks!

0 Kudos
1 Reply

328 Views
Pavel
NXP Employee
NXP Employee

The T2080 PCIe and T1040 PCIe are similar controllers. Do you use the same SDK Linux BSP on the T2080 and T1040 boards?

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos