OHCI context controller active bit doesn't clear

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OHCI context controller active bit doesn't clear

914 次查看
hv
Contributor II

I'm having a problem running on the T2080 that when I transmit to a PCIe by setting the OHCI context controller run bit, the context controller active bit is set and remains set (never clears!)  The active bit is set and cleared only by the Host Controller. 

Can someone tell me why this is the case?  This piece of code runs fine on the T1040.

thanks!

0 项奖励
回复
1 回复

833 次查看
Pavel
NXP Employee
NXP Employee

The T2080 PCIe and T1040 PCIe are similar controllers. Do you use the same SDK Linux BSP on the T2080 and T1040 boards?

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复