Multiple eLBC connections?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple eLBC connections?

1,399件の閲覧回数
toddreed
Contributor I

I assume you can have multiple Enhanced Local Bus Controller connections as there are multiple chip selects?  I am looking to connect two FPGAs on one eLBC.  Are there any reference designs?

Thanks,


Todd

タグ(2)
0 件の賞賛
返信
1 返信

1,335件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes you can have multiple devices connected to the eLBC bus; these devices may share the address/data/controls lines and selected by different chips selects. I do not see what processor and FPGAs you want to connect. So I could not be sure for the reference design. There are reference designs for processor with eLBC which have FPGA and NOR/NAND flashes connected to the eLBC.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信