Multiple eLBC connections?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple eLBC connections?

1,452 Views
toddreed
Contributor I

I assume you can have multiple Enhanced Local Bus Controller connections as there are multiple chip selects?  I am looking to connect two FPGAs on one eLBC.  Are there any reference designs?

Thanks,


Todd

Tags (2)
0 Kudos
Reply
1 Reply

1,388 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes you can have multiple devices connected to the eLBC bus; these devices may share the address/data/controls lines and selected by different chips selects. I do not see what processor and FPGAs you want to connect. So I could not be sure for the reference design. There are reference designs for processor with eLBC which have FPGA and NOR/NAND flashes connected to the eLBC.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply