MicroSD for B4860

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MicroSD for B4860

跳至解决方案
2,326 次查看
TaniaB
Contributor I

What is the maximum size of Micro SD Card that can be used with B4860 processor?

0 项奖励
回复
1 解答
2,317 次查看
Pavel
NXP Employee
NXP Employee

The Section 20.1.1 in the B4860 Reference Manual shows the features of the B4860 eSDHC module:Compatible with the SD memory card specification version 2.0, and supports the high capacity SD memory card.

There is the following information about max capacity for SDHC card in internet:

The Secure Digital High Capacity (SDHC) format, announced in January 2006 and defined in version 2.0 of the SD specification, supports cards with capacities up to 32 GB.

See the following page:

https://en.wikipedia.org/wiki/SD_card

在原帖中查看解决方案

1 回复
2,318 次查看
Pavel
NXP Employee
NXP Employee

The Section 20.1.1 in the B4860 Reference Manual shows the features of the B4860 eSDHC module:Compatible with the SD memory card specification version 2.0, and supports the high capacity SD memory card.

There is the following information about max capacity for SDHC card in internet:

The Secure Digital High Capacity (SDHC) format, announced in January 2006 and defined in version 2.0 of the SD specification, supports cards with capacities up to 32 GB.

See the following page:

https://en.wikipedia.org/wiki/SD_card