MicroSD for B4860

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,282件の閲覧回数
TaniaB
Contributor I

What is the maximum size of Micro SD Card that can be used with B4860 processor?

0 件の賞賛
返信
1 解決策
2,273件の閲覧回数
Pavel
NXP Employee
NXP Employee

The Section 20.1.1 in the B4860 Reference Manual shows the features of the B4860 eSDHC module:Compatible with the SD memory card specification version 2.0, and supports the high capacity SD memory card.

There is the following information about max capacity for SDHC card in internet:

The Secure Digital High Capacity (SDHC) format, announced in January 2006 and defined in version 2.0 of the SD specification, supports cards with capacities up to 32 GB.

See the following page:

https://en.wikipedia.org/wiki/SD_card

元の投稿で解決策を見る

1 返信
2,274件の閲覧回数
Pavel
NXP Employee
NXP Employee

The Section 20.1.1 in the B4860 Reference Manual shows the features of the B4860 eSDHC module:Compatible with the SD memory card specification version 2.0, and supports the high capacity SD memory card.

There is the following information about max capacity for SDHC card in internet:

The Secure Digital High Capacity (SDHC) format, announced in January 2006 and defined in version 2.0 of the SD specification, supports cards with capacities up to 32 GB.

See the following page:

https://en.wikipedia.org/wiki/SD_card