MicroSD for B4860

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MicroSD for B4860

Jump to solution
2,308 Views
TaniaB
Contributor I

What is the maximum size of Micro SD Card that can be used with B4860 processor?

0 Kudos
Reply
1 Solution
2,299 Views
Pavel
NXP Employee
NXP Employee

The Section 20.1.1 in the B4860 Reference Manual shows the features of the B4860 eSDHC module:Compatible with the SD memory card specification version 2.0, and supports the high capacity SD memory card.

There is the following information about max capacity for SDHC card in internet:

The Secure Digital High Capacity (SDHC) format, announced in January 2006 and defined in version 2.0 of the SD specification, supports cards with capacities up to 32 GB.

See the following page:

https://en.wikipedia.org/wiki/SD_card

View solution in original post

1 Reply
2,300 Views
Pavel
NXP Employee
NXP Employee

The Section 20.1.1 in the B4860 Reference Manual shows the features of the B4860 eSDHC module:Compatible with the SD memory card specification version 2.0, and supports the high capacity SD memory card.

There is the following information about max capacity for SDHC card in internet:

The Secure Digital High Capacity (SDHC) format, announced in January 2006 and defined in version 2.0 of the SD specification, supports cards with capacities up to 32 GB.

See the following page:

https://en.wikipedia.org/wiki/SD_card