Linux DPAA driver lacks receive TCP/IP checksum offload

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux DPAA driver lacks receive TCP/IP checksum offload

2,251件の閲覧回数
sebastianhuber
Contributor II

There is no receive TCP/IP checksum offload implemented in the latest DPAA network interface driver for Linux, e.g. git://git.freescale.com/ppc/upstream/linux.git:

grep -r CHECKSUM_ drivers/net/ethernet/freescale/dpaa/

drivers/net/ethernet/freescale/dpaa/dpaa_eth_common.c:  if (skb->ip_summed != CHECKSUM_PARTIAL)

drivers/net/ethernet/freescale/dpaa/dpaa_eth_sg.c: skb->ip_summed = CHECKSUM_NONE;

drivers/net/ethernet/freescale/dpaa/dpaa_eth_sg.c: skb->ip_summed = CHECKSUM_NONE;

Is this the right repository? Is there already an NXP Git repository location?

0 件の賞賛
返信
2 返答(返信)

1,931件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Sebastian Huber,

I checked DPAA related source code in the latest SDK 2.0 release, it seems the attached driver files are very different from yours.

Please try you could access this link http://sw-stash.freescale.net/projects/SDK/repos/linux-sdk2.0/browse .


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,931件の閲覧回数
sebastianhuber
Contributor II

Thanks for your information, however, the specified link is dead.

The attached sources are rather old and the Linux driver of the repository mentioned in my original posting is much newer. It lacks also the receive TCP/IP checksum offload.

Where can I find the latest Linux sources for the QorIQ platform after the NXP takeover of Freescale? What are the plans with respect to pushing the Linux support into the mainline kernel?

0 件の賞賛
返信