Linux DPAA driver lacks receive TCP/IP checksum offload

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linux DPAA driver lacks receive TCP/IP checksum offload

2,253 次查看
sebastianhuber
Contributor II

There is no receive TCP/IP checksum offload implemented in the latest DPAA network interface driver for Linux, e.g. git://git.freescale.com/ppc/upstream/linux.git:

grep -r CHECKSUM_ drivers/net/ethernet/freescale/dpaa/

drivers/net/ethernet/freescale/dpaa/dpaa_eth_common.c:  if (skb->ip_summed != CHECKSUM_PARTIAL)

drivers/net/ethernet/freescale/dpaa/dpaa_eth_sg.c: skb->ip_summed = CHECKSUM_NONE;

drivers/net/ethernet/freescale/dpaa/dpaa_eth_sg.c: skb->ip_summed = CHECKSUM_NONE;

Is this the right repository? Is there already an NXP Git repository location?

0 项奖励
回复
2 回复数

1,933 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Sebastian Huber,

I checked DPAA related source code in the latest SDK 2.0 release, it seems the attached driver files are very different from yours.

Please try you could access this link http://sw-stash.freescale.net/projects/SDK/repos/linux-sdk2.0/browse .


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,933 次查看
sebastianhuber
Contributor II

Thanks for your information, however, the specified link is dead.

The attached sources are rather old and the Linux driver of the repository mentioned in my original posting is much newer. It lacks also the receive TCP/IP checksum offload.

Where can I find the latest Linux sources for the QorIQ platform after the NXP takeover of Freescale? What are the plans with respect to pushing the Linux support into the mainline kernel?

0 项奖励
回复