Layerscape PCIe Endpoint Development Boards

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Layerscape PCIe Endpoint Development Boards

7,855 Views
mikedubya
Contributor I

Are there any NXP or third-party development boards that feature a Layerscape processor such as the LS1021A as a PCIe Endpoint?  All of the NXP development boards focus on the LS processors as PCIe RC.

There is this note here on modifying the LS1046A-RDB board so that mPCIe Slot 2 can be converted from RC to EP mode:

https://community.nxp.com/t5/QorIQ-Knowledge-Base/LS1046A-RDB-in-PCIe-Endpoint-Mode/ta-p/1107415

But even with that change, you would be left with a female mPCIe Slot on the board.  I could not find an adapter that would allow you to connect that mPCIe Slot to a PCIe x1 connector on a desktop PC.

If we wanted to debug a PCIe driver to a Layerscape processor, it would be better to do so on a development board before performing a custom design.

 

0 Kudos
Reply
5 Replies

7,843 Views
mikedubya
Contributor I

Is PCIe EP mode supported on any of the Layerscape processors?  From the KnowledgeBase note, it looks like it is supported on the LS1046.

Related to that, are there any NXP or third-party boards that have a PCIe x1 or x4 interface to a Layerscape processor in PCIe EP mode?

0 Kudos
Reply

7,847 Views
ufedor
NXP Employee
NXP Employee

PCIe EP mode is not supported by LS1021A - refer to the QorIQ LS1021A Reference Manual, 28.2.2 Features:

"Supports Root Complex (RC) mode"

EP mode is not announced.

0 Kudos
Reply

7,842 Views
mikedubya
Contributor I

Is PCIe EP mode supported on any of the Layerscape processors?  From the KnowledgeBase note, it looks like it is supported on the LS1046.

Related to that, are there any NXP or third-party boards that have a PCIe x1 or x4 interface to a Layerscape processor in PCIe EP mode?

0 Kudos
Reply

7,829 Views
mikedubya
Contributor I

Based upon a couple of sources (Table 4 of the Layerscape SDK for Yocto and Linux v5.12-rc7 Documentation/devicetree/bindings/pci/layerscape-pci.txt) it looks like the Layerscape processors that support PCIe EP mode are:

LS1046A
LS1088A
LS2088A
LX2160A (r2)

But I still could not find an NXP or third-party PCIe x1 or x4 development board that exercises this interface.

0 Kudos
Reply

7,818 Views
ufedor
NXP Employee
NXP Employee

I'm not aware about evaluation boards for LS1046A, LS1088A, LS2088A, LX2160A having PCIe EP.

0 Kudos
Reply