LS1046ARDB Fans

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046ARDB Fans

Jump to solution
4,188 Views
matthej
Contributor II

Hi,

 

I was interested in purchasing the LS1046ARDB eval board (already have the FRWY board). On the schematics it lists 5 fan headers (J12, J17, J24, J25 and J502). These headers are located throughout the board (see attached png file).

 

I was wondering if fans do come with this board? If not, are there recommendations on which type of Fans to use (P/N)?

Also, do they connect to the header and sit off the board?

 

Thanks!

 

0 Kudos
Reply
1 Solution
4,177 Views
ufedor
NXP Employee
NXP Employee

On the side of the chassis.

View solution in original post

0 Kudos
Reply
3 Replies
4,184 Views
ufedor
NXP Employee
NXP Employee

LS1046ARDB is provided in the case/box/chassis equipped with fans:

LS1046ARDB.jpg

0 Kudos
Reply
4,181 Views
matthej
Contributor II

Thanks!

 

So just curious, how are they mounted inside the chassis? Are they on the actual PCB board or mounted somehow on the side of the chassis?

 

0 Kudos
Reply
4,178 Views
ufedor
NXP Employee
NXP Employee

On the side of the chassis.

0 Kudos
Reply