LS1046ARDB Fans

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,191件の閲覧回数
matthej
Contributor II

Hi,

 

I was interested in purchasing the LS1046ARDB eval board (already have the FRWY board). On the schematics it lists 5 fan headers (J12, J17, J24, J25 and J502). These headers are located throughout the board (see attached png file).

 

I was wondering if fans do come with this board? If not, are there recommendations on which type of Fans to use (P/N)?

Also, do they connect to the header and sit off the board?

 

Thanks!

 

0 件の賞賛
返信
1 解決策
4,180件の閲覧回数
ufedor
NXP Employee
NXP Employee

On the side of the chassis.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,187件の閲覧回数
ufedor
NXP Employee
NXP Employee

LS1046ARDB is provided in the case/box/chassis equipped with fans:

LS1046ARDB.jpg

0 件の賞賛
返信
4,184件の閲覧回数
matthej
Contributor II

Thanks!

 

So just curious, how are they mounted inside the chassis? Are they on the actual PCB board or mounted somehow on the side of the chassis?

 

0 件の賞賛
返信
4,181件の閲覧回数
ufedor
NXP Employee
NXP Employee

On the side of the chassis.

0 件の賞賛
返信