LS1046A i2c-3 function

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1046A i2c-3 function

295 次查看
Sally_Jay
Contributor I

I cannot scan the device on i2c-3

In dts,the configure is

i2c3: i2c@21b0000 {
compatible = "fsl,vf610-i2c", "fsl,ls1046a-vf610-i2c";
#address-cells = <1>;
#size-cells = <0>;
reg = <0x0 0x21b0000 0x0 0x10000>;
interrupts = <GIC_SPI 59 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clockgen 4 1>;
fsl-scl-gpio = <&gpio3 12 0>;
status = "okay";
};
 
I checked the datasheet
Sally_Jay_0-1757380702535.png

 

Sally_Jay_1-1757380705275.png

 

from the datasheet,it says the default value is 0000_1111h.
I add the bellow command to rcw_1800_qspiboot_1133_5a59.rcw
.pbi
//SCFG_RCWPMUXCR0, configure IIC4_SCL/SDA=000
write 0x157040C, 0x00000000
.end
after I add above command, the device cannot boot up.
I tried 0x00000011, 0x00330000.
all values will cause the device cannot boot.
What value do i need to configure? or I need to do more configure for this function?

0 项奖励
回复
1 回复

238 次查看
yipingwang
NXP TechSupport
NXP TechSupport
0 项奖励
回复