LS1046A USB2_DRVVBUS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1046A USB2_DRVVBUS

跳至解决方案
2,135 次查看
tian_shuliang
Contributor I

We use ls1046a to design a board refer to frwy-ls1046a-ac, USB2_DRVVBUS is low level since the USB initialization, USB_DRVVBUS is high. 

I want to know why USB2_DRVVBUS is low when usb initialization?

0 项奖励
回复
1 解答
2,048 次查看
Pavel
NXP Employee
NXP Employee

Check that pin multiplexing is correct on your board. See the IIC3_SCL in the SCFG_RCWPMUXCR0 register.

Check your command sequence using the Section 34.4.3.1 and the Table 34-9 from the LS1046A Reference Manual:

https://www.nxp.com/webapp/Download?colCode=LS1046ARM

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,049 次查看
Pavel
NXP Employee
NXP Employee

Check that pin multiplexing is correct on your board. See the IIC3_SCL in the SCFG_RCWPMUXCR0 register.

Check your command sequence using the Section 34.4.3.1 and the Table 34-9 from the LS1046A Reference Manual:

https://www.nxp.com/webapp/Download?colCode=LS1046ARM

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复