LS1046A USB2_DRVVBUS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A USB2_DRVVBUS

Jump to solution
2,134 Views
tian_shuliang
Contributor I

We use ls1046a to design a board refer to frwy-ls1046a-ac, USB2_DRVVBUS is low level since the USB initialization, USB_DRVVBUS is high. 

I want to know why USB2_DRVVBUS is low when usb initialization?

0 Kudos
Reply
1 Solution
2,047 Views
Pavel
NXP Employee
NXP Employee

Check that pin multiplexing is correct on your board. See the IIC3_SCL in the SCFG_RCWPMUXCR0 register.

Check your command sequence using the Section 34.4.3.1 and the Table 34-9 from the LS1046A Reference Manual:

https://www.nxp.com/webapp/Download?colCode=LS1046ARM

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,048 Views
Pavel
NXP Employee
NXP Employee

Check that pin multiplexing is correct on your board. See the IIC3_SCL in the SCFG_RCWPMUXCR0 register.

Check your command sequence using the Section 34.4.3.1 and the Table 34-9 from the LS1046A Reference Manual:

https://www.nxp.com/webapp/Download?colCode=LS1046ARM

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply