LS1046A PCIE failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A PCIE failed

1,698 Views
wong
Contributor I

ls1046a 配置PCIE,系统正常启动,但是PCIE功能好像不对。

RCW 配置如下:

SRDS_PRTCL_S1=13107  // 0X3333
SRDS_PRTCL_S2=23129  // 0X5A59
SRDS_REFCLK_SEL_S1=0
SRDS_REFCLK_SEL_S2=0
SRDS_PLL_PD_S1=2
SRDS_PLL_PD_S2=0

 

uboot下查看pci,无信息。

=> pci 1
No such bus
pci 2
No such bus
=> pci 3
No such bus
=> pci 4
No such bus
=> pci 5
No such bus

 

启动内核时打印pcie信息:RC 显示no link

PCIe1: pcie@3400000 Root Complex: no link
PCIe2: pcie@3500000 disabled
PCIe3: pcie@3600000 Root Complex: no link

 

使用lspci 工具查看没有找到外部pcie设备。

wong_1-1723018636390.png

 

附件是完整的log记录。麻烦帮忙分析哪里存在问题。

 

 

 

 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,635 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please check PLL mapping SRDS_PLL_REF_CLK_SEL_S2

Please check whether the following configuration is suitable for your custom board.

* Serdes 2:
* PLL mapping: 2221
* SRDS_PLL_REF_CLK_SEL_S2 : 0b'00
* SerDes 2, PLL1[162] : 0 - 100MHz for SATA
* SerDes 2, PLL2[163] : 0 - 100MHz for PCIe

0 Kudos
Reply