LS1043ARDB boot from eMMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043ARDB boot from eMMC

ソリューションへジャンプ
2,774件の閲覧回数
CurtisChen
Contributor I

Hi,

     We plan to remove QSPI flash and use emmc only on our LS1043ARDB product, but I don't found u-boot config (ls1043ardb_emmc_defconfig) in LSDK 18.12.

     May I know LS1043ARDB can boot from emmc in LSDK 18.12?

     If it supported, could you guide me how to build emmc image of u-boot?

 

      Thanks 

タグ(2)
0 件の賞賛
返信
1 解決策
2,769件の閲覧回数
ufedor
NXP Employee
NXP Employee

LSDK 18.12 is out-of-date - please use LSDK 20.12

LS1043A supports booting from eMMC.

There is no "ls1043ardb_emmc_defconfig" because LS1043ARDB does not possess an eMMC device.

The "ls1043ardb_sdcard_defconfig" and "ls1046ardb_emmc_defconfig" can be used as references for "ls1043ardb_emmc_defconfig".

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,770件の閲覧回数
ufedor
NXP Employee
NXP Employee

LSDK 18.12 is out-of-date - please use LSDK 20.12

LS1043A supports booting from eMMC.

There is no "ls1043ardb_emmc_defconfig" because LS1043ARDB does not possess an eMMC device.

The "ls1043ardb_sdcard_defconfig" and "ls1046ardb_emmc_defconfig" can be used as references for "ls1043ardb_emmc_defconfig".

0 件の賞賛
返信