LS1043ARDB boot from eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043ARDB boot from eMMC

Jump to solution
2,763 Views
CurtisChen
Contributor I

Hi,

     We plan to remove QSPI flash and use emmc only on our LS1043ARDB product, but I don't found u-boot config (ls1043ardb_emmc_defconfig) in LSDK 18.12.

     May I know LS1043ARDB can boot from emmc in LSDK 18.12?

     If it supported, could you guide me how to build emmc image of u-boot?

 

      Thanks 

Tags (2)
0 Kudos
Reply
1 Solution
2,758 Views
ufedor
NXP Employee
NXP Employee

LSDK 18.12 is out-of-date - please use LSDK 20.12

LS1043A supports booting from eMMC.

There is no "ls1043ardb_emmc_defconfig" because LS1043ARDB does not possess an eMMC device.

The "ls1043ardb_sdcard_defconfig" and "ls1046ardb_emmc_defconfig" can be used as references for "ls1043ardb_emmc_defconfig".

View solution in original post

0 Kudos
Reply
1 Reply
2,759 Views
ufedor
NXP Employee
NXP Employee

LSDK 18.12 is out-of-date - please use LSDK 20.12

LS1043A supports booting from eMMC.

There is no "ls1043ardb_emmc_defconfig" because LS1043ARDB does not possess an eMMC device.

The "ls1043ardb_sdcard_defconfig" and "ls1046ardb_emmc_defconfig" can be used as references for "ls1043ardb_emmc_defconfig".

0 Kudos
Reply