LS1043ARDB CWTAP connection failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043ARDB CWTAP connection failed

4,248 Views
lingguan
Contributor II

Hi,

I cannot connect LS1043ARDB by using CodeWarrior TAP and CWH-CTP-CTX10-YE.

The error:

pastedImage_1.png

How to solve this problem? Maybe I am not configure SW correctly?

Sincerely.

0 Kudos
Reply
5 Replies

4,084 Views
Pavel
NXP Employee
NXP Employee

Is there log from CCS if connection is not happen?


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:

This thread is continued as a private discussion with the submitter,
NXP support is not following the thread anymore.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,080 Views
Pavel
NXP Employee
NXP Employee

Your dump shows that there is connection between CodeWarrior TAP and your board. CodeWarrior TAP has read ID and detected the LS1043a rev1.x.

 

See attached snapshot. Check CodeWarrior setting using this snapshot.

Attached file also contains simple CodeWarrior project for the LS1043ARDB board.


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:

This thread is continued as a private discussion with the submitter,
NXP support is not following the thread anymore.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,080 Views
lingguan
Contributor II

I refer to your method but the problem is still exist.

Sometimes CCS can not find the device.

Sincerely.

0 Kudos
Reply

4,080 Views
Pavel
NXP Employee
NXP Employee

Check JTAG connection on your board using the Figure 100 of the LS1043a Datasheet:

https://www.nxp.com/webapp/Download?colCode=LS1043A

 

Test your connection to your board using the following commands in CCS:

config cc cwtap

show cc

 

and

 

log v

source IDcode.tcl

 

See the following page:

https://community.nxp.com/docs/DOC-94804


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,080 Views
lingguan
Contributor II

Thanks for your reply.

I use CCS and test my connection:

pastedImage_1.png

I just set SW3[6] = 1 for JTAG configuration. LS1043ARDB, CWTAP and CWH-CTP-CTX10-YE are all new, so the pyhsical connection really have some errors?

Sincerely.

0 Kudos
Reply