Is QorIQ LS1021A-IOT Reference Design still supported ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is QorIQ LS1021A-IOT Reference Design still supported ?

351 Views
danny30
Contributor I

Hi, 

Is LS1021A-IOT reference design still supported by NXP ? The linux build system is in this repo iiot-gateway · GitHub (user guide pdf)

but many others referenced in this build system were removed, eg: https://github.com/iiot-gateway/nxp-ZigbeeDemo 

If it is not being supported what is the recommended reference design now ?

Thanks !

0 Kudos
1 Reply

295 Views
alexander_yakov
NXP Employee
NXP Employee

Our current SDK for Layerscape processors supports only one LS1021A-based board - TWR-LS1021A

So, I recommend using this board in order to be supported by this Layerscape SDK.

Here is a direct link to "Supported Targets" page in Layerscape SDK documentation:

https://nxp.sdlproducts.com/LiveContent/content/en-US/LSDKUG_Rev19.03/GUID-81326FC4-0F5E-4BFB-AA35-9...


Have a great day,
Alexander,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos