LS1043A QSPI Boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,839件の閲覧回数
j_wallace
Contributor II

Hi Experts,

We are designing custom LS1043A based bord that will boot from QSPI NOR flash. When I build u-boot from DENX u-boot-fsl-qoriq for LS1043AQDS board it looks like there is no SPL build. So I would like to ask

1) How does the QSPI boot work? How code gets from QSPI NOR flash to SDRAM?

Furthermore, I saw that SPI MTD driver is also linked to u-boot when building for LS1043AQDS and this driver does not seem to support the QSPI flash of our custom board. So perhaps we will have to patch the driver to match our device.

2) Is MTD driver involved in the boot process for QSPI boot?

Thanks in advance.

0 件の賞賛
返信
1 解決策
3,099件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the following document:

https://community.nxp.com/docs/DOC-102040

 

This document shows that QSPI NOR Flash is used as memory-mapped flash.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,100件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the following document:

https://community.nxp.com/docs/DOC-102040

 

This document shows that QSPI NOR Flash is used as memory-mapped flash.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,099件の閲覧回数
j_wallace
Contributor II

Ok,

Thanks for your feedback.

Best regards.

0 件の賞賛
返信