LS1043A JTAG Programming Connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A JTAG Programming Connection

3,078 Views
logeshs
Contributor II

Hi,

We are using LS1043A. I kindly request you to suggest us

1. what programmer should be used for programming LS1043A?

2. Programmer's operating Voltage level

3. Mating Connector part number of that programmer so that we can use it in our board.

4. Also if you have any datasheet for the programmer i request you to share the same to us.

Thanks.

0 Kudos
Reply
6 Replies

2,848 Views
ufedor
NXP Employee
NXP Employee

The request is not clear.

What exactly do you mean by "programming LS1043A"?

Which board is in question?

0 Kudos
Reply

2,848 Views
logeshs
Contributor II

The question is about JTAG Configuration Signals Connector, Standard Cortex Debug Connector given in Figure.99 of LS1043A datasheet.

0 Kudos
Reply

2,848 Views
ufedor
NXP Employee
NXP Employee

The header part number is Samtec FTSH-105-01-L-DV.

Other questions about "programmer" still are not clear.

Do you mean "debugger"?

If "yes", then refer to the following links:

CodeWarrior ARMv8 64 bit|NXP 

CodeWarrior TAP|NXP 

0 Kudos
Reply

2,848 Views
logeshs
Contributor II

Yes, I mean about Debugger.

0 Kudos
Reply

2,848 Views
logeshs
Contributor II

As per Figure.100 in LS1043A datasheet VDD is connected to 1.8V. Please confirm does the debugger supports/operates in 1.8V?

0 Kudos
Reply

2,848 Views
ufedor
NXP Employee
NXP Employee

CoreWarrior TAP supports JTAG operation at 1.8V.

0 Kudos
Reply