Hello,
Could anybody toggle I2C pins on LS1026 during JTAG test?
These are not toggling in my board while in operational mode all is ok to all I2C devices.
Thanks,
Itzik
解決済! 解決策の投稿を見る。
The test engineer found the solution:
Not like the LS1046, the LS1026 I2C/UART Power Bank need to be Configured before it can be used in JTAG Mode, so added extra command before each test that use this Power Bank.
The test engineer found the solution:
Not like the LS1046, the LS1026 I2C/UART Power Bank need to be Configured before it can be used in JTAG Mode, so added extra command before each test that use this Power Bank.
Test other pins on your LS1026a board. Perhaps there are a few similar pins on your board.
If the LS1026a I2C correctly works in normal mode, your JTAG test setting should be checked.
Other bus like DDR, SPI are function OK in JTAG
Only problem with DVDD pins (I2C, UART)
Pins have been verified , we have checked with a scope and found pins are not toggling at all in JTAG Mode while other pins are toggling.
I2C pins are working fine in normal mode.