LS1012AXN7EKB Processor is not booting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1012AXN7EKB Processor is not booting

12,450 次查看
vlakshmanan
Contributor I

Dear sir

 

We are using LS1012A in one of My projects.

We are facing a booting issue.

The processor reads the 64 Bytes data from Flash Memory (PN : S25FS512SAGMFI011 ) . Afterward the PBI Initialization is not happened.

We cannot see the DDR Clocks and clock from CLK_OUT pin from the processor.

Hence, we are suspecting the Platform clock switching is not happened.

Here I am attaching the Schematics for your reference.

Please find the attachments and help us to resolve the issues.

 

Thanks, and Regards,

Lakshmanan V

0 项奖励
回复
11 回复数

12,445 次查看
ufedor
NXP Employee
NXP Employee

1) Check POR voltage at QSPI_A_DATA1 - it is recommended to use 4.7kOhm pull-down resistor.

2) What is the POR voltage at QSPI_A_DATA0?

3) What is the POR voltage at UART1_SOUT?

4) Please provide dump of the first 64 bytes of the SPI Flash.

5) What is measured SD_REF_CLK frequency?

0 项奖励
回复

12,425 次查看
vlakshmanan
Contributor I

Hello sir,

 

1) Check POR voltage at QSPI_A_DATA1 - it is recommended to use 4.7kOhm pull-down resistor.

We replaced to 4.7K pull-down resistor. But no improvement.

2) What is the POR voltage at QSPI_A_DATA0?

We measured 1.8V POR voltage at QSPI_A_DATA0  pin

3) What is the POR voltage at UART1_SOUT?

We measured 1.8V POR voltage at UART1_SOUT pin

4) Please provide dump of the first 64 bytes of the SPI Flash.

For your reference I am attaching RCW_PBL_DATA image.

5) What is measured SD_REF_CLK frequency?

SD1_REF_CLK1_P/N pull-down to ground. We are not giving any clock input to this pin.

-------------------------------------------------------------------------------------------------------------------------

 

While measuring QSPI_A_DATA3 pin we are getting always 1.8 Volts.

For Hard-coded RCW mode we grounded CLK_OUT pin at POR, Hard-coded RCW mode not working.

Please give me the solution as soon as possible.

 

Regards

Lakshmanan V

 

 

0 项奖励
回复

12,420 次查看
ufedor
NXP Employee
NXP Employee

Please provide binary image of the RCW.

0 项奖励
回复

12,416 次查看
vlakshmanan
Contributor I

Hello sir,

 

             Hereby I am enclosed binary image of the RCW.

This is the serious issue for us. So please give the solution as soon as possible.

 

Regards

Lakshmanan V

0 项奖励
回复

12,406 次查看
ufedor
NXP Employee
NXP Employee

You wrote:

> Afterward the PBI Initialization is not happened

Provided RCW is correct "by itself" - i.e. it has correct CRC, but there is no PBI section containing code to be loaded into the OCRAM.

Also in the RCW there is following PBI:

00 02 00 00 58 01 57 09

after swapping:

09 57 01 58 00 00 02 00 - load 0x200 into Alternate CBAR register (ALTCBAR)

What is your intention?

 

Please consider using Layerscape SDK to build composite firmware image.

You can refer to pre-built firmware image at:

https://lsdk.github.io/components.html

LSDK IMAGES, select 2004 in the drop-down.

 

0 项奖励
回复

12,398 次查看
vlakshmanan
Contributor I

Hello sir,

 

we have followed this procedure and built the "flexbuild_lsdk2004_update_290520" in ubuntu and generated the file "bl2_qspi.pbl".

But the problem is we are unable to flash the QSPI through the CWTAP. As we have previously mentioned that the hard-coded RCW mode did not work for us, and the QSPI flash program window did not open and it opened for the FRWY-LS1012a EVM board which we have.

We are waiting for the valuable feedback.

 

Regards

Lakshmanan V

 

0 项奖励
回复

12,392 次查看
ufedor
NXP Employee
NXP Employee

You have to refer to the LSDK Documentation and build composite firmware image:

https://docs.nxp.com/bundle/GUID-51EEFEDB-ABD5-40C0-BEBD-6527B3494D57/page/GUID-47B8F1F5-3A8F-45F4-A...

Resulting firmware image has to be programmed into SPI Flash.

 

> we are unable to flash the QSPI through the CWTAP

How the RCW was programmed?

0 项奖励
回复

12,382 次查看
vlakshmanan
Contributor I

Hello sir,

 

we are unable to flash the QSPI through the CWTAP

                  As we mentioned in the previous mail that the hard-coded RCW mode did not work for us.Due to this QSPI flash program window did not open for us.

We are waiting for the valuable feedback.

 

Regards

Lakshmanan V

 

0 项奖励
回复

12,376 次查看
ufedor
NXP Employee
NXP Employee

> we are unable to flash the QSPI through the CWTAP

How the RCW was programmed?

0 项奖励
回复

12,330 次查看
vlakshmanan
Contributor I

Hello sir,

 

                         RCW was not programmed in QSPI. Because of both QSPI  RCW mode and Hard-coded RCW mode is not working.

 

Regards

Lakshmanan V

0 项奖励
回复

12,324 次查看
ufedor
NXP Employee
NXP Employee

Originally you wrote:

> The processor reads the 64 Bytes data from Flash Memory

Have you tried to connect CodeWarrior using "USE_SAFE_RCW = True"?

Refer to the CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA, Targeting Manual, 8.6.1 RCW Override.

0 项奖励
回复