LS1012 USB1_VBUS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012 USB1_VBUS

2,163件の閲覧回数
philbaron
Contributor I

What is the maximum tolerated voltage on the USB1_VBUS (pin 4) on the LS1012. Datasheets seems to imply that it is part of the 1.8V bank, but eval boards have this pin connected directly to VBUS which is 5V.

0 件の賞賛
返信
2 返答(返信)

2,094件の閲覧回数
Bulat
NXP Employee
NXP Employee

USB1_VBUS is not a power pin, it is an input signal with nominal voltage of 5V. Please see the AN5192 for details.

Regards,

Bulat

0 件の賞賛
返信

2,093件の閲覧回数
philbaron
Contributor I

Bulat,

Thanks for the quick and concise response.

Phil Baron

Aeronix Inc.

777 Lowndes Hill Rd.

Bldg 3, Suite 160

Greenville, SC 29607

864-250-1950 x258

0 件の賞賛
返信