JTAG!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
3,274 次查看
qammarabbas
Contributor IV

Hi,

I am interfacing DDR3L and NOR Flashes with T1042. Both of these external devices does not support JTAG. Does it mean i cannot use the JTAG feature of T1042 to test the connectivity on the board? What are the functions of JTAG other than checking connectivity?

标记 (1)
1 解答
2,913 次查看
alexander_yakov
NXP Employee
NXP Employee

JTAG interface in T1042 is not only boundary scan interface, but also debug interface - debugger can be connected to that interface and execute code on target processor under debugger control. Using this method, you can test your DDR memory by bringing up processor' DDR controller and executing memory test code. Also, this JTAG debug interface is used to execute Flash Programmer code at target processor for in-system NOR flash programming.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
2,914 次查看
alexander_yakov
NXP Employee
NXP Employee

JTAG interface in T1042 is not only boundary scan interface, but also debug interface - debugger can be connected to that interface and execute code on target processor under debugger control. Using this method, you can test your DDR memory by bringing up processor' DDR controller and executing memory test code. Also, this JTAG debug interface is used to execute Flash Programmer code at target processor for in-system NOR flash programming.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,913 次查看
qammarabbas
Contributor IV

Thanks!

Could you please tell me which JTAG connector should i use with T1042? The COP connector or the Aurora? 

0 项奖励
回复
2,913 次查看
alexander_yakov
NXP Employee
NXP Employee

JTAG connector is sometimes mentioned as "COP" or "JTAG/COP" because debig interface connecter over standart JTAG interface is named "COP". Aurora is another, high speed debug interface.

0 项奖励
回复